Hi all,
The driver and fw version is lf-5.15.71_2.2.0
After firmware load the driver reports with
[ 94.244794] Fail to poll firmware status: firmwarestat=0x5f5f
I did some modification to the driver and found that the firmwarestat initially comes back 0xf00a before settling on 0x5f5f
I'd like to know exactly what this means so I can diagnose why my driver is failing to get past the firmware load.
What I need is register definitions for the status_reg_0 and status_reg_1, or at least the meaning of 5f5f and f00a
Hi,
Could you please help me with the following information?
- What host are you using?
- Are you using a module?
- Please share with me the FW (i.e. 17.92.1.p149.131) and Driver (i.e. MM6X17437.p3-GPL) version
- Please share with me the whole terminal output of your test
Regards,
Daniel.
host is an stm32mp133 soc
yes the module is a u-blox maya-w166
firmware and driver version are both lf-5.15.71_2.2.0
I have tried lf-6.6.23_2.0.0 but no difference
Full output is
# modprobe moal mod_para=nxp/wifi_mod_para.conf
[ 70.725070] mlan: loading out-of-tree module taints kernel.
[ 70.859894] wlan: Loading MWLAN driver
[ 70.862830] wlan: Register to Bus Driver...
[ 70.869680] vendor=0x02DF device=0x9159 class=0 function=1
[ 70.873902] Attach moal handle ops, card interface type: 0x108
[ 70.887336] SDIW416: init module param from usr cfg
[ 70.890831] card_type: SDIW416, config block: 0
[ 70.895396] cfg80211_wext=0xf
[ 70.902521] max_vir_bss=1
[ 70.903992] cal_data_cfg=none
[ 70.911343] ps_mode = 1
[ 70.912607] auto_ds = 1
[ 70.915041] host_mlme=enable
[ 70.921864] fw_name=nxp/sdiouartiw416_combo_v0.bin
[ 70.925568] SDIO: max_segs=341 max_seg_size=131040
[ 70.933368] rx_work=0 cpu_num=1
[ 70.935197] Attach mlan adapter operations.card_type is 0x108.
[ 70.944556] wlan: Enable TX SG mode
[ 70.948777] wlan: Enable RX SG mode
[ 70.958168] Request firmware: nxp/sdiouartiw416_combo_v0.bin
[ 71.259021] Wlan: FW download over, firmwarelen=534196 downloaded 534196
[ 74.256252] Fail to poll firmware status: firmwarestat=0x5f5f
[ 74.260646] FW failed to be active in time!
[ 74.264819] wlan_dnld_fw fail ret=0xffffffff
[ 74.274195] WLAN: Fail download FW with nowwait: 0
[ 74.279665] SDIO Func0 (0x0-0x9): 43 03 02 02 03 00 00 02 03 00
[ 74.284455] SDIO Func1 (0x10-0x17): 00 00 00 00 ff ff ff ff
[ 74.293079] SDIO Func1: (0x8) 00 (0x58) 00 (0x5c) 08 (0x5d) 00 (0x60) 07 (0x61) 0c (0x62) 00 (0x64) 10 (0x65) 00 (0x66) 00 (0x68) 00 (0x69) 00 (0x6a) 00
[ 74.316762] SDIO Func1 (0xe8-0xf2): 5f 5f 08 00 05 02 08 00 24 14 70
[ 74.424442] SDIO Func1 (0xe8-0xf2): 5f 5f 08 00 05 02 08 00 24 14 70
[ 74.429803] woal_request_fw failed
[ 74.432856] Firmware Init Failed
[ 74.440741] Free module params
[ 74.442422] woal_add_card failed
[ 74.446103] wlan_sdio: probe of mmc0:0001:1 failed with error -1
[ 74.458360] wlan: Register to Bus Driver Done
[ 74.461345] wlan: Driver loaded successfully
Thanks for the information.
I just did a test on my side using 1XK module with an iMX8MP EVK and it is working on my side in Linux 5.15.71.
imx8mpevk login: root
root@imx8mpevk:~# clear
root@imx8mpevk:~# modprobe moal mod_para=nxp/wifi_mod_para.conf
[ 29.265837] mlan: loading out-of-tree module taints kernel.
[ 29.291622] wlan: Loading MWLAN driver
[ 29.295727] wlan: Register to Bus Driver...
[ 29.300097] vendor=0x02DF device=0x9159 class=0 function=1
[ 29.305668] Attach moal handle ops, card interface type: 0x108
[ 29.312528] SDIW416: init module param from usr cfg
[ 29.317469] card_type: SDIW416, config block: 0
[ 29.322081] cfg80211_wext=0xf
[ 29.325051] max_vir_bss=1
[ 29.327684] cal_data_cfg=none
[ 29.330664] ps_mode = 1
[ 29.333111] auto_ds = 1
[ 29.335568] host_mlme=enable
[ 29.338460] fw_name=nxp/sdiouartiw416_combo_v0.bin
[ 29.343276] SDIO: max_segs=128 max_seg_size=65535
[ 29.347989] rx_work=1 cpu_num=4
[ 29.351159] Attach mlan adapter operations.card_type is 0x108.
[ 29.357334] wlan: Enable TX SG mode
[ 29.360845] wlan: Enable RX SG mode
[ 29.365836] Request firmware: nxp/sdiouartiw416_combo_v0.bin
[ 29.612519] Wlan: FW download over, firmwarelen=534196 downloaded 534196
[ 30.882123] WLAN FW is active
[ 30.885105] on_time is 30883373750
[ 30.910641] fw_cap_info=0x187c4f03, dev_cap_mask=0xffffffff
[ 30.916264] max_p2p_conn = 8, max_sta_conn = 8
[ 30.932033] Register NXP 802.11 Adapter mlan0
[ 30.937986] Register NXP 802.11 Adapter uap0
[ 30.945449] Register NXP 802.11 Adapter wfd0
[ 30.953892] wlan: version = SDIW416---16.92.21.p55.3-MM5X16366.p5-GPL-(FP92)
[ 30.962991] wlan: Register to Bus Driver Done
[ 30.967473] wlan: Driver loaded successfully
root@imx8mpevk:~# uname -r
5.15.71+g95448dd0dc9b
root@imx8mpevk:~#
Are you using a custom board for the Host? Have you double checked if a HW rework is needed on your board?
Regards,
Daniel.
Yes this is a custom board, and it may be true that some power up conditions are not 100% true to the datasheet.
But...
It would be really helpful to get the meanings of those firmwarestat values though, if at all possible.
"firmwarestat=0x5f5f" and f00a
After all, they must have a specific meaning within the module/chipset itself
Could you please take a look this thread? Seems like a similar issue.
Please share with me your wifi_mod_para.conf
Regards,
Daniel.
This is the config file
I know it works because the firmware load works on some prototype boards but fail on some others
SDIW416 = {
cfg80211_wext=0xf
max_vir_bss=1
cal_data_cfg=none
ps_mode=1
auto_ds=1
host_mlme=1
fw_name=nxp/sdiouartiw416_combo_v0.bin
}
Would still love to know what those firmwarestat values mean
Hi @vmbtech,
Please confirm the following.
1. The log you attached is with 5.15.71 driver (SDIW416---16.92.21.p55.3-MM5X16366.p5-GPL-(FP92)) in Linux 5.15.71.
2. If you do not modify the driver, you only get 0x5f5f. But if you modify the driver, you get the same 0x5f5f value, but you notice that 0xf00a appears first, am I right?
Regards,
Daniel.
I will need to check this internally.
Give me some time to get an update.
Regards,
Daniel.