Hello,
I am evaluating energy harvesting function on OM2NTP5332 board,I am testing the OM2NTP5332 board with App "NTAG5 - Dev. kit Use Cases", after sending some commands to the board,Output voltage only 0.176V.using App "Xplore NTAG 5",Output voltage only 0.176V.
Is there any way to restore the circuit board so that the Vout voltage output can be configured to 2.5V? thanks!
Hello @liyidreamer .
Please kindly refer to the 4.2.8 EH & ED settings of the UM11207 as the link.
URL:https://www.nxp.com.cn/docs/en/user-guide/UM11207.pdf.
Have a nice day.
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-----------------------------------------------------------------------------