MKW41Z register RSIM->CONTROL requires reading GENFSK register first

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MKW41Z register RSIM->CONTROL requires reading GENFSK register first

778 次查看
gauthier_osterv
Contributor I

I am having trouble reading the RF_OSC_READY field of RSIM->CONTROL.

I noticed my firmware unexpectedly reports that the oscillator is not ready if I check like this:

if (!(RSIM->CONTROL & RSIM_CONTROL_RF_OSC_READY_MASK)) {
    return RADIO_RESULT_ERROR; /* Error, OSCERCLK is not running! */
}

However, reading a register from the GENFSK module solves the issue, and RSIM->CONTROL reports RF_OSC_READY as expected:

+ volatile uint32_t dummy_read; 
+
+ /* RSIM control does not have OSC_READY if we don't make this read
+ first. It's unclear if it's a problem with the RSIM register updating its
+ value, or the clock actually not starting without the read. Read of any
+ GENFSK register makes it work (actually only tested with
+ GENFSK->NTW_ADR_0 besides PACKET_CFG). */
+ dummy_read = GENFSK->PACKET_CFG;
+
 if (!(RSIM->CONTROL & RSIM_CONTROL_RF_OSC_READY_MASK)) {
     return RADIO_RESULT_ERROR; /* Error, OSCERCLK is not running! */
 }


Is this known behavior? Should I do it another way? My guess is that the oscillator is ready although the register reports it isn't, is it the case?

标签 (2)
标记 (2)
1 回复

638 次查看
estephania_mart
NXP TechSupport
NXP TechSupport

Hello, 

We usually recommend using the available API's in the SDK to make easier the development of your own application.

I would recommend you to check the rf_osc_startup function available in I believe all the examples on the SDK  which just give you our implementation of what you are trying to achieve, you can find it in the fsl_xcvr.c file. 

Regards, 

Estephania 

0 项奖励
回复