Hi,
I am trying to write data to MF DESFire EV 1 card over RF, but I am having a problem. When I send update binary command I am getting 6700 wrong length error. Here is update binary command;
03 00 D6 00 02 05 54 02 65 6E 31
Could anyone help me?
Hi @zafer2021 ,
Mifare Desfire EV1 command information is available in the data sheet , but not allowed to discuss here as it is under NDA. You may request from the NXP doc store with a valid NDA. Please kindly refer to the attachment for more details.
Have a great day,
Kan
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------