LF RF communication FXTH870xD - MRB-KW019030JA

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LF RF communication FXTH870xD - MRB-KW019030JA

1,308 Views
dskim
Contributor I

I'm using MRB-KW019030JA with (MKW01_IAR7v4_Project_TPMS_Rev0.6) project, also I have FXTH870xD sensor module But I recently realized that MRB-KW019030, MRB-KW019032 has different crystal.

MRB-KW019030 has 30Mhz and the other has 32Mhz.

unfortunately the project recommand KW019032 and I have only KW019030 I have no idea how to modify the source code I just found this

//#define USE_32MHZ_CLKO //Enable this macro when using a 32MHZ crystal fed to the MKW01Z128CHN
#define USE_30MHZ_CLKO //Enable this macro when using a 30MHz crystal fed to the MKW01Z128CHN

in derivative.h so I fix it to 30Mhz 

could somebody tell me how to fix this code more to fit on my MRB-KW019030?

Labels (1)
0 Kudos
Reply
2 Replies

1,065 Views
dskim
Contributor I

Hi Tomnas,

The project name is TPMS MKW01 Reference Project LF RF Communication KDS3 not MKW01_IAR7v4_Project_TPMS_Rev0.6

it was my mistake

you can download project here Search Results: TPMS MKW01 Reference Project LF RF Communication KDS3 

Thankyou

0 Kudos
Reply

1,065 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi  Daeseon,

Please check the attached project and let me know if it helps you.

Best regards,

Tomas

0 Kudos
Reply