KW41Z supports up to 2 simultaneous connections in hardware.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

KW41Z supports up to 2 simultaneous connections in hardware.

778件の閲覧回数
seanwu
Contributor IV

Dear sir,

The description in KW41Z datasheet:

Bluetooth v4.2 Low Energy compliant 1 Mbps GFSK modulation supporting up to 2 simultaneous connections in hardware.

What does this mean?

It means when KW41Z is a central role, it just can connect to 2 peripherals simultaneously, right?

If KW41Z is a peripheral role, could it connect to 2 other device(central or peripheral) simultaneously?

THanks.

BR,

Sean

kw41z ble 802.15.4 kinetis kw41‌

ラベル(2)
0 件の賞賛
返信
1 返信

483件の閲覧回数
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi Seanwu,

The kw41 supports both roles as central (connect 2 peripheral simultaneous) or 2 other device(central or peripheral) simultaneously.

Best Regards,

Mario