JN516x ZigBee Home Automation SDK?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

JN516x ZigBee Home Automation SDK?

2,096 Views
pahanela
Contributor II

I am currently evaluating JN5168 as component for integration project which involves communication over ZigBee in Home Automation profile.

On the page ZigBee Home Automation|NXP there are broken links to JN516x ZigBee Home Automation SDK and BeyondStudio for NXP​. Is there alternative place where I can get this information?

Tags (2)
6 Replies

1,408 Views
hwolf
Contributor I

you can visit :  ZigBee家庭自动化|恩智浦,   this is a right site! I checked it .

0 Kudos
Reply

1,408 Views
hamidjabbar
Contributor I

You Can download this file from

MEGA

Hamid

0 Kudos
Reply

1,408 Views
vicentegomez
NXP TechSupport
NXP TechSupport

Hi

Do you still have the problem?

Regards

Vicente Gomez

0 Kudos
Reply

1,408 Views
pahanela
Contributor II

Yes.

0 Kudos
Reply

1,408 Views
vivekpjohn
Contributor II

Hai,

Yes i am still having the problem. How to rectify this issue?

--

सादर / With Warm Regards,

विवेक फिलिप जॉन/Vivek Philip John

अभियंता/Engineer

ईडीसी- एम्बेडेड सिस्टम्स/EDC- Embedded Systems

भारत हेवी इलेक्ट्रिकल्स लिमिटेड/Bharat Heavy Electricals Limited

बॉयलर ऑग्जिलरीज प्लांट रानीपेट /Boiler Auxiliaries Plant -Ranipet

तमिलनाडु/Tamilnadu – 632406 , भारत/India

दूरभाष/Ph:04172-284136

मोबाइल/Mobile: 75985 35723

Quoting vicentegomez <admin@community.freescale.com>:

Pedro Vicente Gomez Salazar

replied to the discussion

"JN516x ZigBee Home Automation SDK?"

To view the discussion, visit:

https://community.nxp.com/message/810801?et=watches.email.thread#comment-810801

>

0 Kudos
Reply

1,408 Views
vivekpjohn
Contributor II

hi

i am also facing the same issue

0 Kudos
Reply