JN5168 sleep mode

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

JN5168 sleep mode

521 Views
29603655
Contributor I

Hello:

  I use the function vAHI_Sleep(E_AHI_SLEEP_OSCON_RAMON) to let MCU enter sleep mode, but it always enter program mode when it wakeup. I check that because I use the SPIMISO pin as button, when JN5168 wakeup and the button press at the same time it will enter program mode.

  So how to disable JN5168 wake up from boot phase.

Thanks

BR

0 Kudos
Reply
1 Reply

406 Views
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi Liang,

To avoid programming mode: leave pin floating high during reset to avoid entering UART. 

If that specific pin is used for a button, you could try to connect to high.

Please let me know your findings.

Regards,

Mario

0 Kudos
Reply