I am trying to setup the develoment software for Zigbee 3.0 development.
And got everything thing up and running but when importing the ZigBee 3.0 Base Device Template / Light Bulbs. something goes wrong and it wont import the source files only the .cproject an .project files are copied to the workspace.
I am following the manual JN-UG-3098 2.2 Importing a project.
I must be making a very simple mistake here but i can't seem to figure it out.
Hey Mario,
Yep i managed to import and compile.
The current problem is that i cant seem to find how to generate the ZPS Configuration files.
I have the plugin installed and made an edit to the JN-AN-1218 but how do i go from the app.zpscfg to the .c/h files, the documentation speeks about an command line tool but nowhere (that i can find) in the documentation is mentioned how to invoke that tool.
Hi Youp,
The zpscfg file will create a zps_gen.c/h file, and for example, if you add the endpoint number 1, the zps will define an endpoint number 1.
.zpscfg file
zps_gen.h
The App_dimmablelight.c will use this define
PUBLIC uint8 app_u8GetDeviceEndpoint( void)
{
return DIMMABLELIGHT_LIGHT_ENDPOINT;
}
and the makefile has defined the zps_gen.c
APPSRC += zps_gen.c
I am not sure if this what you are asking.
Please let me know.
Regards,
Mario
Hi Mario,
Thanks for you help, I figured it out when you press comiple the zps_gen files gets updated and that wasn't clear to me.
But after the compile I see the changes that where made to the files.
Thank you very much.
Hi Mario,
That is one of the first places I looked but did not help me. But I found in the JN-AN-1218 a document with a hint in how to solve it.
The key step for me was putting all the files in the work space before trying to import, I don't know why this differs from the manuals but I got it working.
But I now I am looking into using the JN-AN-1218, I compiled it without much trouble for the JN5168 module that I have.
It wont connect to the Philips Hue bridge after power up, did not figure out why yet. but I could connect via the TouchLink method.
So now I am looking in to editing the example. I made some changes to the app.zpscfg with the ZPS Configurator plugin. But now where in the manual is specified how I generate the source/header files from the app.zpscfg, I did read on the this forum that you have to use the make file for it. but where can I find that make file, because the JN-AN-1218 makefile doesn't seem to generate the new configuration files form app.zpscfg.
Hi Youp,
I'm sorry, I am following your question, Did you solved your issue?
Please let me know if you have any further question.
Regards,
Mario
Hi Youp,
Please look at the next community post.
https://community.nxp.com/docs/DOC-340028
Regards,
Mario