The RAM of JN5189 has two areas, RAM0 (88KB) and RAM1 (64KB), but when I compile official Demos (such as JN-AN-1244), only RAM0 is used, even if the amount of memory consumed exceeds the size of RAM0, it will not RAM1 will be used, so I want to know how to use RAM1? Or which document introduces this content? I did not find it.
Thank you very much!
Hi,
Customer can try to use second 64KB RAM partition by define variables of following way:
uint8_t temp[1024] __attribute__ ((section(".bss.$RAM2")));
Regards,
Mario