HTRC110 FILTERL not working with HITAG 2

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

HTRC110 FILTERL not working with HITAG 2

232 Views
PreyerM
Contributor I

Hi,

I‘m using HTRC110 to communicate vis RFID with Hitag and Hitag 2 using standard configuration settings which work fine except for Hitag2 with response frequency of 4 kHz. The answer from the transponder is recognized 1 out if 10 reading attempts. We found out it has to do with low pass filter set to 3 kHz, FILTERL= 0 = 3 kHz. But when changing to FILTERL= 1 = 6 kHz there is no recognition of any transponder. Actually switching off the low pass filter via DISLP1 it is working better.

Wuestion: Are there known bugs regarding setting FILTERL= 1 = 6 kHz? Is there a workaround except DISLP1=1? Is there other possibility to boost transponder recognition?

Tags (2)
0 Kudos
Reply
0 Replies