The FW crashed issue is still exist in Generic_PCIE-WLAN-UART-BT-8997-LNX_6_6_3-IMX8-16.92.21.p119.2-16.92.21.p119.2-MM6X16437.P3-GPL.
follow previous case:
and reopen by this case.
Hi, @ArthurC
Thanks for your quick reply.
We have Linux 5.15.71_2.2.2, Linux 5.15.71_2.2.1 and Linux 5.15.71_2.2.0 prebuilt image versions on our website.
Please share the exact version of the 8MQ pre-built image that you have flashed to avoid any discrepancy.
Thanks,
Christine.
Hello @Christine_Li,
Please use command "dkpg install" to install the network manager package in official prebuild image.
And then nmcli will be working.
Please use the prebuilt image "imx-image-full-imx8mqevk.wic" to test.
Thank you.
Hi, @ArthurC
We checked the zip file shared by the customer, it only contains .deb files, we need an executable nmcli binary which we can directly copy to 8MQ and use. Can you please share it to us?
Also, We have Linux 5.15.71_2.2.2, Linux 5.15.71_2.2.1 and Linux 5.15.71_2.2.0 prebuilt image versions on our website. Please share the exact version of the 8MQ pre-built image that you have flashed to avoid any discrepancy.
Best regards,
Christine.
Hello @Christine_Li,
We are using (standalone prebuilt image + your yocto build nmcli binary) to test.
But our EVK's PMIC (pfuse100) is unexpected broken during the test procedure.
Probably it was purchased for long time ago. It can't boot anymore.
So we can't provide the results for you.
The yocto build nmcli binary is as attached.
Please help to use it to check.
Thank you
Hi, @ArthurC
Thanks for your quick reply.
1. If you have complete BSP(i.MX8MQ-EVK prebuilt image + nmcli package) then please provide us the full BSP image.
2. If you are using the (standalone prebuilt image + your yocto build nmcli binary) then please provide us the nmcli binary to install in our i.MX8MQ-EVK and also provide the steps which you followed to install the nmcli binary in our i.MX8MQ-EVK.
Best regards,
Christine.
Hi, @ArthurC
Thanks for your feedback.
I know you mentioned that you are using nmcli on your 8MQ board. And also you mentioned same issue can be reproduced on our 8MQ-EVK + our prebuilt image.
Can you please help to confirm on our 8MQ-EVK + our pre-built image what did you use?
nmcli or wpa_supplicant ?
Best regards,
Christine.
Hello @Christine_Li,
Yes, will provide the setup flow to you based on EVK later.
Actually, there are a lots of unexpect risks during shipping the product to you.
So dealing with issue based on EVK will be better.
Thank you for your help.
Will provide to you next Thursday.
Hi, @ArthurC
I know you mentioned that you are using nmcli on your 8MQ board. And also you mentioned same issue can be reproduced on our 8MQ-EVK + our prebuilt image.
Can you please help to confirm on our 8MQ-EVK + our pre-built image what did you use?
nmcli or wpa_supplicant ?
We are still trying to reproduce on our locally. Thanks for your understanding.
Best regards,
Christine.
Hi, @ArthurC
I am so sorry, I am from TIC wireless connectivity team. According to our company's policy, I am only allowed to provide online support for mass market customers. So I am not allowed to have a business trip to your office.
So please help to prepare the board and send to us so that we can capture requested logs and move forward. We have tried one week to try to reproduce, but unfortunately we could not reproduce locally right now. So we sincerely ask for your help. Please understand us. Without your help and the logs, we stuck here, could not move forward.
Best regards,
Christine.
Hello @Christine_Li,
Have you got any chance to prepare the test environment(your Image / some test script) on the board?
-> No, I need to deal with lots of other work assigned by Tony.
Have you sent out the board to me?
-> No, because there are lots progresses needed to follow in GIGABYTE.
Please let me know the status of delivery so that I can track where it is.
Could you have a business trip to our office to capture the logs locally without product sending?
Hi, @ArthurC
Thank you for the feedback.
I saw your supervisor has approved to send us one of your board.
Have you got any chance to prepare the test environment(your Image / some test script) on the board? Please help to sync the test steps with your previous test and make sure we can reproduce on this board with less operations.
Please let me know when can you send out and share me the delivery number so that we can track further.
Thanks for your efforts and corporations.
Best regards,
Christine.
Hello @Christine_Li ,
Can you please help to get the answers of the below queries?
1. Is DUT BT is mater or slave?
-> Master.
2. Is DUT BT is source or sink?
-> Source.
3. Which BT reference device(remote BT headset) are you using for the test?
-> FiiO BTR3
Hi, @ArthurC
Can you please help to get the answers of the below queries?
1. Is DUT BT is master or slave?
2. Is DUT BT is source or sink?
3. Which BT reference device(remote BT headset) are you using for the test? Can you please help to provide model and version?
Best regards,
Christine.
Hello @Christine_Li,
I don't have permission about sending our product to you.
Please send mail to my supervisor according the following mail address:
Hi, @ArthurC
Yes, I know. During the test, we keep the Wi-Fi connection in 2.4G, and the PC which is doing iperf also connected to the same 2.4G AP. Bluetooth is playing A2DP music under 3M baud rate.
So please help also to check on your side whether is possible to send one of your board with your setup, so that we can reproduce and capture related logs. Without your help, it is too difficult for us to proceed further.
Best regards,
Christine.
Hello @Christine_Li ,
Please make sure the Wi-Fi connection is under 2.4 GHz & play bluetooth audio in the same time in 88W8997.
If it is in 5GHz. The issue will not be occured.
Please fix the AP is 2.4GHz or set PC working under 2.4GHz in direct connection.