What is the operating lifetime (service time) of the Vybrid?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

What is the operating lifetime (service time) of the Vybrid?

974 Views
vadimaleynikov
Contributor III

What is the Vybrid expected service time, i.e. how long can the Vybrid operate under Operating ratings?

Labels (1)
Tags (1)
2 Replies

659 Views
b36401
NXP Employee
NXP Employee

Officially the lifetime is 62831 hours at max junction temperature. It means about 7 hears.
However lifetime depends on the temperature.
Please refer the picture I attached. It shows the de-rating of lifetime relative to junction temperature.
It is not really reliability information for 100% POH, but it tells you what the estimated lifetime will be, in power-on hours, depending on junction temperature.

Have a great day,
Victor

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

659 Views
vadimaleynikov
Contributor III

Hello Victor,

Thank you very much for your reply.

Best regards,

Vadim

0 Kudos
Reply