Vybrid (vf610) Chip Errata document

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Vybrid (vf610) Chip Errata document

2,366 次查看
lukaszmajewski
Contributor III

Dear Community,

I would like to ask if there is a "Chip errata" document for Vybrid (e.g. vf610)?

I'm asking since there are some issues with DMA usage with DSPI controller and also QSPI controller HW issues as pointed out in the Linux kernel code:

(What's more is that there is a bug in  the "IP Command Read" in the Vybrid.) found here:
 https://elixir.bootlin.com/linux/v4.19-rc4/source/drivers/mtd/spi-nor/fsl-quadspi.c#L671

I've found some Vybrid errata: https://www.nxp.com/docs/en/errata/VYBRID_2N02G.pdf 

but it seems a bit outdated now. It also doesn't provide information, which I need.

For example - the iMX6Q has a very detailed (and up to date) "Chip Errata" document:

标签 (3)
标记 (2)
1 回复

2,065 次查看
lukaszmajewski
Contributor III

Could anybody from NXP comment on this issue?

Thanks in advance,

Łukasz