How many QSPI ports does the VF6 have? Can they be used simultaneously?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How many QSPI ports does the VF6 have? Can they be used simultaneously?

Jump to solution
776 Views
flaviocaduda
Contributor II

In the document AN4947 - Understanding Vybrid Architecture, figure 1, depicts a QuadSPI-0 and a QuadSPI-1. I could not find within the documentation much information on the QuadSPI-1. The idea is to use the QuadSPI-0 as an interface for 2 serial flash, while the QuadSPI-1 as an interface for a FPGA.

Can both QSPI-0 & QSPI-1 be used simultaneously? Are there any restrictions? Any special considerations when using QSPI-1?

Regards,

Flavio

Labels (1)
0 Kudos
Reply
1 Solution
556 Views
naoumgitnik
Senior Contributor V

Dear Flavio!

Please, take a look at the Re: Parallel QuadSPI and Re: Can Vybrid boot from the only QSPI_B? threads and let me know if you still have any questions.

Attached is also an excerpt from one of the Freescale designs with 3 QuadSPI (QSPI) memory chips used.

Sincerely, Naoum Gitnik.

View solution in original post

0 Kudos
Reply
2 Replies
557 Views
naoumgitnik
Senior Contributor V

Dear Flavio!

Please, take a look at the Re: Parallel QuadSPI and Re: Can Vybrid boot from the only QSPI_B? threads and let me know if you still have any questions.

Attached is also an excerpt from one of the Freescale designs with 3 QuadSPI (QSPI) memory chips used.

Sincerely, Naoum Gitnik.

0 Kudos
Reply
556 Views
flaviocaduda
Contributor II

Thank you Naoum!

0 Kudos
Reply