edge-aligned setting in kinetis k40

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

edge-aligned setting in kinetis k40

3,160件の閲覧回数
MatteoPioTotta
Contributor I

Hi,i need to set edge-aligned pwm in kinetis k40 but i can't understand how set 'COMBINE'=0 MSnB=1 and CPWMS=0. I already set DECAPEN and QUADEN using the mask,but i can't set COMBINE,MSnB AND CPWMS!Anyone can help me?

タグ(4)
0 件の賞賛
返信
3 返答(返信)

2,525件の閲覧回数
admin
Specialist II

Are you setting the WPDIS?  (Write Protect Disable)

If that doesn't fix it send the snippet of your code where your initializing the FTM.

0 件の賞賛
返信

2,525件の閲覧回数
MatteoPioTotta
Contributor I

Hi,

i'm a student and i 'm reading a dc motor tutorial of k40.I already set Write Protect Disable as wrote in tutorial but i can understand how set decapen msnb and combine using the mask.

0 件の賞賛
返信

2,525件の閲覧回数
MatteoPioTotta
Contributor I

My code is:

/*

* PWM.c

*

*  Created on: 10/set/2012

*      Author: teteo

*/

#include "Clock.h"

#include"derivative.h"

#include<stdio.h>

float MotorTickVar;

void InizializzazionePwmMotore() 

{

    //Enable the Clock to the FTM1 Module

    SIM_SCGC6 |= SIM_SCGC6_FTM1_MASK;

    // PORTC_PCR4 = PORT_PCR_MUX(1) | PORT_PCR_DSE_MASK;   //Enable GPIO on on the pin -

    //route the output of that channel 0 to the pin... (pick a different multiplexer value for routing the timer)

    //ch 11.4.1 of the k40 reference manual is the pin control register

    //For port c pin 1..   bits 10-8  Pin Mux Control...

    PORTA_PCR8  = PORT_PCR_MUX(3)  | PORT_PCR_DSE_MASK;

    PORTA_PCR9  = PORT_PCR_MUX(3)  | PORT_PCR_DSE_MASK;

    // Choose EDGE-Aligned PWM:  selected when QUADEN=0, DECAPEN=0, COMBINE=0, CPWMS=0, and MSnB=1  (page 964)

    // Properly set up Flex Timer Module

    ////Per prima cosa bisogna abilitare la scrittura di alcuni registri:

    //FTM0_MODE[WPDIS] = 1; //Disable Write Protection - enables changes to QUADEN, DECAPEN, etc. 

    FTM1_MODE |= FTM_MODE_WPDIS_MASK;//DISABILITA LA PROTEZIONE DELLA SCRITTURA

    /////////////////SETTAGGIO DECAPEN

   

    //FTMEN is bit 0, need to set to zero so DECAPEN can be set to 0

    FTM1_MODE &= ~1; //METTE A ZERO DECAPEN

    

    /////////////SETTAGGIO QUADEN

   

    //Set Edge Aligned PWM

    FTM1_QDCTRL &=~FTM_QDCTRL_QUADEN_MASK; 

    //QUADEN is Bit 1, Set Quadrature Decoder Mode (QUADEN) Enable to 0,   (disabled)

    //FTM0_SC = 0x16; //Center Aligned PWM Select = 0, sets FTM Counter to operate in up counting mode,

    //it is field 5 of FTMx_SC (status control) - also setting the pre-scale bits here

  //////PROVO A SETTARE DECAPEN E COMBINE

   

    FTM1_COMBINE|=FTM_COMBINE_COMBINE0_MASK;

    FTM1_/////////???????????????????????????

   

   

   

    //   Also need to setup the FTM0C0SC channel control register  - Page 897   section 37.3.6

  FTM1_CNT = 0x0; //FTM Counter Value - (initialize the CNT before writing to MOD)  (16 bit available - bits 0-15 are count)

  FTM1_MOD = 0x0; //Set the Modulo register (16 bit available - bits 0-15), Mod is set to 24000

  FTM1_CNTIN = 0; //Set the Counter Initial Value to 0   (pg 915)

  //change MSnB = 1

  FTM1_C0SC |= FTM_CnSC_ELSB_MASK;

  FTM1_C0SC &= ~FTM_CnSC_ELSA_MASK;

  FTM1_C0SC |= FTM_CnSC_MSB_MASK;

  FTM1_C0V = 0x0; //Set the Channel n Value to  (16 bit available - bits 0-15)

  //Set the complimentary pinout

  FTM1_C1SC |= FTM_CnSC_ELSB_MASK;

  FTM1_C1SC &= ~FTM_CnSC_ELSA_MASK;

  FTM1_C1SC |= FTM_CnSC_MSB_MASK;

  FTM1_C1V = 0x0;

  FTM1_SC = FTM_SC_PS(0) | FTM_SC_CLKS(1); 

  // Interrupts

  FTM1_SC |= FTM_SC_TOIE_MASK; //enable the interrupt mask

  enable_irq(63);  // (79-16) Set NVIC location, but you still have to change/check NVIC file sysinit.c under Project Settings Folder

}

// Set the PWM of the Motor

void SetMotorPWM(float DutyCycle)

{

   //float compDuty = (float)100.0-DutyCycle;

   FTM1_C0V =(int)((DutyCycle*.01)* (float)0x0);

   FTM1_C1V =(int)((1.0-DutyCycle*.01)* (float)0x0);

}

//Create Interrupt when motor functions are complete

void MotorTick()

{

if (MotorTickVar < 0xff)//if motor tick less than 255 count up...

   MotorTickVar++;

//Clear the overflow mask if set

   if(FTM1_SC & FTM_SC_TOF_MASK)

   FTM1_SC &= ~FTM_SC_TOF_MASK;

   //LED_E2_TOGGLE; // ends up being ___ Hz (correct)

}

0 件の賞賛
返信