What machine have select in environment setup for T2081 for the linux sdk to enter into U-boot?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

What machine have select in environment setup for T2081 for the linux sdk to enter into U-boot?

619 次查看
Vimalprasad
Contributor II

I have downloaded  QorIQ_SDK-V2.0-20160527-yocto.iso and QorIQ_Linux_SDK_v2.0-1703.tar.bz2 from the Linux_SDK_for_QorIQ_Processors . 

I have installed this files in my system by following the documentation QorIQ-SDK-2.0-1703.

I have to setup the environment for the T2081 processor.  for setup the machine I have to give the command to select one which is supported for T2081 processor.

 

$ . ./fsl-setup-env -m <machine>
For example:
$ . ./fsl-setup-env -m b4860qds-64b
The following shows the usage text for the fsl-setup-env command:
Usage:
$ . ./fsl-setup-env -h
Usage: . fsl-setup-env -m <machine>
Supported machines
QorIQ: b4420qds-64b b4420qds b4860qds-64b b4860qds c293pcie ls1021atwr ls1043ardb p2041rdb
p3041ds p4080ds p5020ds-64b p5020ds p5040ds-64b p5040ds t1023rdb-64b t1023rdb t1024rdb-64b t1024rdb
t1040d4rdb-64b t1040d4rdb t1042d4rdb-64b t1042d4rdb t2080qds-64b t2080qds t2080rdb-64b t2080rdb
t4160qds-64b t4160qds t4240qds-64b t4240qds t4240rdb-64b t4240rdb ls1012afrdm-32b ls1012afrdm
ls1012ardb-32b ls1012ardb ls1043ardb-32b ls1046ardb-32b ls1046ardb ls2088ardb

 

I can't find which type of machine have to select for my T2081 processor.Can you please tell which machine need to select?

 

0 项奖励
回复
1 回复

584 次查看
June_Lu
NXP TechSupport
NXP TechSupport

T2080xxx would be recommended.
Select T2080RDB and T2080QDS which one will be more similar function to the customer board.

0 项奖励
回复