Flashing 8-bit NOR on T1042 Based Board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Flashing 8-bit NOR on T1042 Based Board

Jump to solution
943 Views
EmbEng
Contributor III

We are trying to bring-up T1042 based custom board with an 8-bit NOR  flash attached on CS0 of IFC interface. We have modified the .tcl configuration file to configure IFC for 8-bit flash. While trying to program the NOR flash using PA Flash Programmer Task, we are getting following errors in CodeWarrior console for 'Diagnostics' action:

fl::target -lc "Debugging_Part2-core00_RAM_T1042_Connect"
fl::target -b 0x0 0x40000
fl::target -v off -l off
cmdwin::fl::device -d "MT28EW01GABA1HPC" -o "128Mx8x1" -a 0xe8000000 0xefffffff
cmdwin::fl::diagnose
 Beginning Operation ...    
------------------------- 
Performing target initialization ...    
 Downloading Flash Diagnostics Driver ...   
 Reading flash ID ...
Running Diagnostics ...   
Error:  The Diagnostics operation failed.   Flash diagnostics reports the following error(s):  Operation Unsupported
Error:  Diagnose operation failed
Error: The Diagnostics operation failed. Flash diagnostics reports the following error(s):  Operation Unsupported

And following while running 'Program and Verify' action:

fl::target -lc "Debugging_Part2-core00_RAM_T1042_Connect"
fl::target -b 0x0 0x40000
fl::target -v off -l off
cmdwin::fl::device -d "MT28EW01GABA1HPC" -o "128Mx8x1" -a 0xe8000000 0xefffffff
cmdwin::fl::image -f "C:\\Users\\Admin\\Desktop\\rcw_1400MHz.bin" -t "Binary/Raw Format" -re on -r 0xe8000000 0xefffffff -oe off
cmdwin::fl::write
------------------------- 
Using restricted address range 0xE8000000 to 0xEFFFFFFF   
Programming file C:\Users\Admin\Desktop\rcw_1400MHz.bin   
 0 Bytes Programmed, Check Restricted Address Range   
Program Command Succeeded   
cmdwin::fl::image -f "C:\\Users\\Admin\\Desktop\\rcw_1400MHz.bin" -t "Auto Detect" -re on -r 0xe8000000 0xefffffff -oe off
cmdwin::fl::verify
------------------------- 
Using restricted address range 0xE8000000 to 0xEFFFFFFF   
Verifying file C:\Users\Admin\Desktop\rcw_1400MHz.bin   
Auto-detection is successful.   
  File is of type Binary/Raw Format.   
 
0 Bytes Verified, Check Restricted Address Range   
Verify Command Succeeded

Can someone suggest what might be the reason we are unable to diagnose & program flash?

Labels (1)
Tags (2)
0 Kudos
1 Solution
725 Views
ufedor
NXP Employee
NXP Employee

Quality of the processor picture is bad, but it looks like the NOR Flash data lines are connected in a wrong way.

Please consider that in the QorIQ T1040 Reference Manual, 24.9.6 Interfacing to different port sizes it is written:

"A 16-bit port must reside on AD[0:15], and an 8-bit port on AD[0:7]."

View solution in original post

6 Replies
725 Views
ufedor
NXP Employee
NXP Employee

Please provide additional information:

1) processor to flash connection schematics (PDF)

2) ensure that offset value is 0xe8000000 in the Program Action

0 Kudos
725 Views
EmbEng
Contributor III

Thanks for replay ufedor‌.

1) processor to flash connection schematics (PDF)

Sorry I was unable to find PDF attachment option in reply so attaching schematic images below.03.IFC_Interface.jpg

04.NOR_FLASH.jpg

2) ensure that offset value is 0xe8000000 in the Program Action

Adding 0xe8000000 offset in program action results in following CodeWarrior log:

fl::target -lc "Debugging_Part2-core00_RAM_T1042_Connect"
fl::target -b 0x0 0x40000
fl::target -v on -l off
cmdwin::fl::device -d "MT28EW01GABA1HPC" -o "128Mx8x1" -a 0xe8000000 0xefffffff
cmdwin::fl::image -f "C:\\Users\\Admin\\Desktop\\rcw_1400MHz.bin" -t "Binary/Raw Format" -re on -r 0xe8000000 0xefffffff -oe on -o 0xe8000000
cmdwin::fl::write
 Beginning Operation ...    
------------------------- 
Using restricted address range 0xE8000000 to 0xEFFFFFFF   
Programming file C:\Users\Admin\Desktop\rcw_1400MHz.bin   
Performing target initialization ...    
 Downloading Flash Device Driver ...   
 Reading flash ID ...
Downloading 0x00000060 bytes to be programmed at 0xE8000000   
Executing program ....   
Executing program .....   
Executing program ......   
Executing program .......   
Executing program ........   
Executing program .........   
Executing program ..........   
Executing program ...........   

The 'Executing program' message never stops and keeps running. I was also wondering  why Using restricted address range 0xE8000000 to 0xEFFFFFFF message is appearing in log.

0 Kudos
726 Views
ufedor
NXP Employee
NXP Employee

Quality of the processor picture is bad, but it looks like the NOR Flash data lines are connected in a wrong way.

Please consider that in the QorIQ T1040 Reference Manual, 24.9.6 Interfacing to different port sizes it is written:

"A 16-bit port must reside on AD[0:15], and an 8-bit port on AD[0:7]."

725 Views
EmbEng
Contributor III

Do you mean we needed to route IFC AD[0:7] to NOR data port instead of IFC AD[8:15]? If yes, is there any way to swap the byte order of IFC using some register configuration?

0 Kudos
725 Views
ufedor
NXP Employee
NXP Employee

Yes and there is no way to correct the issue programmatically.

0 Kudos
725 Views
EmbEng
Contributor III

Thanks alot for your support ufedor‌. We will try to find some workaround.

0 Kudos