Urgent! CW v5.2 license failed issue!

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Urgent! CW v5.2 license failed issue!

745 次查看
minjie
Contributor I

Dear,

I've try to register the codewarrior license for CW v5.2.But it made error as below picture when I open the CW-HCS12X: CodeWarrior® Development Studio for HCS12(X) Microcontrollers (Classic IDE) v5.2.

The worse is the maximum number of returns is reached.So I really need your help.Appreciation for your feedback!

173808_173808.pngpastedImage_2.png

标签 (1)
0 项奖励
回复
1 回复

495 次查看
stanish
NXP Employee
NXP Employee

Hi,

It seems you are using a floating license.

Have you setup the licensing server and/or updated the server side license?

If your licensing server is up and running and the license.dat  file on the server side includes the license to this CodeWarrior I'd sugest to check if you are able to connect to the licensing server from your client machine:

You can use e.g. telnet and create a TCP connection to the server "MYPC001" default port is 1700.

If you cannot connect I'd suspect that your firewall is blocking the connection.

Stan

0 项奖励
回复