fxls90322实际测试到的加速度值与预期值差异比较大

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

fxls90322实际测试到的加速度值与预期值差异比较大

475 次查看
shanY1
Contributor I
 

1705572600070.png

Y轴加速度值是-0.4g   量程是150g
 
 

1705572987948.png

 

X轴加速度值是3.9g   量程是15.5g
 
1705573630172.png

 

手册推荐的贴装图
 
微信图片_20240118183123.jpg

 

 
X轴
 

微信图片_20240118183132.jpg

Y轴
 
问题描述:
把板子沿X轴或者Y轴进行翻转90度,X轴量程是15.5g,翻转90度之后加速度值是3.9g,Y轴量程是150g,翻转90度之后加速值是0.4g,按照手册的贴装图,沿X轴或Y轴进行90度翻转,加速度应该在+-1g左右。实际测试到的加速度值与预期值差异比较大。
0 项奖励
回复
2 回复数

357 次查看
shanY1
Contributor I

图1中的中文是:Y轴加速度值是-0.4g   量程是150g   图2中的中文是:X轴加速度值是3.9g   量程是15.5g

0 项奖励
回复

454 次查看
JozefKozon
NXP TechSupport
NXP TechSupport

Dear Yakai,

JozefKozon_1-1705656998302.png

Could you please translate the sentences in your pictures? I do not speak Chinese. For the text I use the Google translator, but I cannot translate sentences in the picture.

With Best Regards,

Jozef

 

 

0 项奖励
回复