crystal specification for NTM88

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

crystal specification for NTM88

576件の閲覧回数
Pranav_Tonape
Contributor I

hi NXP,

i have some doute for part selection for TPMS system as follows:

1) at how much PPM 26 MHz crystal we can used ? any documentation if we have please share me.

0 件の賞賛
返信
3 返答(返信)

555件の閲覧回数
JozefKozon
NXP TechSupport
NXP TechSupport

Hi Pranav,

for the recommended Crystal, please refer to the schematic of our EVB attached. EXS00A-CS07225 is used.

JozefKozon_0-1708061609615.png

With Best Regards, 

Jozef

0 件の賞賛
返信

571件の閲覧回数
stephen378baker
Contributor I

Hello Dog Likes Best@Pranav_Tonape 
According to the NTM88 data sheet, the recommended crystal specification for the NTM88 tire pressure sensor family is as follows:

  • Frequency: 26 MHz
  • Frequency tolerance: ±10 ppm
  • Load capacitance: 8 pF
  • Equivalent series resistance: ≤ 40 Ω
  • Drive level: ≤ 100 μW

You can find more information about the NTM88 features and applications in the data sheet and the product page. You can also ask questions and get answers from the NXP community in the Sensors forum.

I hope this answers your question. 


Best Regards
stephen378baker

538件の閲覧回数
Pranav_Tonape
Contributor I
hi Stephen baker,
thanks for replying me, based on your answer i have following query:
1) what is the maximum frequency tolerance is acceptable for NTM88?
2) and if i increase the frequency tolerance what would be the effect we will obvers with NTM88 application and performance wise while other parameter is keeping same?
3) what is the maximum Load capacitance is acceptable for NTM88?
4) and if i increase the Load capacitance what would be the effect we will obvers with NTM88 application and performance wise other parameter is keeping same?
5) what is the maximum Equivalent series resistance is acceptable for NTM88 ?
6) and if i increase the Equivalent series resistance what would be the effect we will obvers with NTM88 application and performance wise other parameter is keeping same?

Thanks and regards,
Pranav Tonape

0 件の賞賛
返信