Hi
I've a question concerning the Demo applikation "ZSTARLIB_EXAMPLE". I can successfully compile and run the app. , but i get no data from my sensors. It seems that no event callback is triggert?
I've not changed anything in the demo source.
The zstarlib.dll is included.
I can see that the com. port is successful opened and i can query the rssi for the first sensor, but i do not get burstdata? or any other event from the API.
Are ther any newer Version of the demo app available?
Are there any special commands/methods which have to be called to get the sensors working?
If i run the "Zstar_Demo" app. i can see the sensor data, and everything works well?
I'm using VS 2008 SR1 with .net 3.5 SR1
thx for your help
Mario