TSUP on MM912J637

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

TSUP on MM912J637

Jump to solution
1,615 Views
igw
Contributor II

Hello all,

The MM912J637 has a low current voltage output intended to drive an external temperature sensor, TSUP, as well as a dedicated ADC.

The specs for TSUP show a +/-5% variation around the nominal 1.25V.

I am wondering if I need to account for this voltage tolerance in my temperature accuracy calculations *or* if the TSUP voltage is related to the ADC's VREF.

So, in effect my question is, is the ADC doing a ratiometric or absolute measurement on the voltage at VTEMP.

How closely does TSUP track VREF is probably the most telling specification (and is not in the datasheet)?

Thanks,

Ian

Labels (1)
0 Kudos
Reply
1 Solution
1,197 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello Ian,

The reference of the External Temp Sensor is TSUP.

This means that for external temperature measurement the variation of TSUP will not impact the measurement.

Regards,

Tomas

View solution in original post

0 Kudos
Reply
1 Reply
1,198 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello Ian,

The reference of the External Temp Sensor is TSUP.

This means that for external temperature measurement the variation of TSUP will not impact the measurement.

Regards,

Tomas

0 Kudos
Reply