Please tell me about MMA8452Q.3-axis, I set the threshold.To sleep.It will wake up when moved.Can I use such a method?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Please tell me about MMA8452Q.3-axis, I set the threshold.To sleep.It will wake up when moved.Can I use such a method?

710 Views
ryosuke
Contributor I

Please tell me about MMA8452Q.3-axis, I set the threshold.To sleep.It will wake up when moved.Can I use such a method?

Labels (1)
Tags (1)
0 Kudos
1 Reply

326 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Roysuke,

Yes, I would recommend you to take a closer look at our AN4074 which explains how to use the Auto-Wake/Sleep feature including example register settings and code.

Attached you can also find my example code written for the FRDM-KL25Z board. The transient function is used to wake up the MMA8451Q and the time-out period is set to 5s.

I hope it helps.

Best regards,

Tomas

PS: If my answer helps to solve your question, please mark it as "Correct". Thank you.

0 Kudos