Media Resistant Gel on MPXA6115AC6U

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Media Resistant Gel on MPXA6115AC6U

1,634件の閲覧回数
erichnast
Contributor I

I see that the MPXAZ6115A is now obsolete, but there is an identical part the MPXA6115AC6U.

One difference from the data sheet is the MPXAZ6115A  has media resistant gel and the MPXA6115AC6U does not.


What is the purpose/function of the media resistant gel?

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

1,047件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Erich,

From the MPXAZ6115A series, the following packaged options are still available as shown on the MPXx6115 Buy/Parametrics website:

MPXAZ6115AC6T1

MPXAZ6115AP

MPXAZ6115APT1 


MPXAZ6115A Availability.JPG.jpg


Their media resistant gel die coat and durable polymer package provide an improved media resistant barrier that allows the sensor to operate reliably in high humidity conditions as well as environments containing common automotive media. More information can be found in this discussion.


Regards,

Tomas


PS: If my answer helps to solve your question, please mark it as "Correct" or “Helpful”. Thank you.

0 件の賞賛
返信