MPXV7007DP stability issue with nothing connected to P1 & P2 ports

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPXV7007DP stability issue with nothing connected to P1 & P2 ports

886 Views
vp
Contributor I

On a MPXV7007DP I connected pin 2 (Vs) to 3.3v. Pin 3 to Ground, and Pin 4 (Vout) to a ADC input pin on a ESP32 m/c.
By simply doing a analogRead() in a loop on a ESP32, i get initial readings of 2050 approx, which are about what they should be, as the two P1 & P2 ports are not connected to anything, so no pressure difference.

However after about a minute the Vout values start decreasing over a span of couple of minutes and then seem to stabilize around 800. This shouldn't happen. The Vout should stay around 2050..

Another observation, if I power down the system for about 5 seconds, and reconnect, Vout remains at 800 approx. If i power it down for 30mins, the then start up, Vout is 2050 for about 30 seconds...

I tried this with two MPXV7007DP chips. One connected just by itself and the other had the filtering capacitors on as described in the datasheet. Both have the same issue.

Whats the fix ? What am I doing wrong ? 

Cheers,

vp

0 Kudos
1 Reply

865 Views
JozefKozon
NXP TechSupport
NXP TechSupport

Dear V P,

could you please test to remove the ESP32 ADC and measure the output directly on the pin 4 Vout with an oscilloscope? To make sure, that the issue is causing our MPXV7007DP and not the ESP32. The MPXV7007DP should also work with 3.3V supply voltage, but recommended supply voltage is 5V. Just for the test could you please connect 5V to the pin 2 Vs? If both ports are unconnected, the differential pressure is 0kPa.

For the supply voltage Vs=3.3V, the output voltage should be

Vout=Vs*(0.057*P+0.5)=3.3*(0.057*0+0.5)=3.3*0.5
Vout=1.65V +/- ERROR

For the supply voltage Vs=5V
Vout=Vs*(0.057*P+0.5)=5*(0.057*0+0.5)=5*0.5
Vout=2.5V +/- ERROR

Are the values 2050 and 800 output voltage in mV?

With Best Regards,

Jozef

0 Kudos