MMA8451Q I2C maximum speed

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MMA8451Q I2C maximum speed

1,484 Views
johncampbell
Contributor II

It's stated on the first page of the Rev10 datasheet the following:

I2C digital output interface (operates to 2.25 MHz with 4.7 kΩ pullup)

Within Section 2.3 table 4 I2C (slave timing values) for SCL clock Low of 1.3 uS and SCL clock High of 600nS.

These are the minimum values.

This implies a maximum clock period of  1.9uS or a Clock speed of 526KHz if you use the minimum time allowed for high and low.

This doesn't correspond to 2.25MHz.

Question1:   What am I missing?

Question 2:   If my micro can support higher I2C rates what is the maximum clock I can run?

Labels (1)
0 Kudos
Reply
4 Replies

1,230 Views
david_diaz
NXP Employee
NXP Employee

Hello John,

Thank you for writing.

In this case, the MMA8451Q supports the I2C Fast Mode, which means that the bidirectional data transfers can be made at up to 400 kbit/s.

The tHIGH and tLOW parameters, are the minimum time in order to perform a correct communication as shown in the image below.

timing.jpg

 

So, the maximum clock you may run using your MCU as a master is 400 kbit/s.

Please let me know if my answer is clear.

Regards,

David

0 Kudos
Reply

1,230 Views
johncampbell
Contributor II

David,

Thanks for your response.

The timing is the standard timing found in the I2C specification.

I would still like to know why it states in the datasheet.

I2C digital output interface (operates to 2.25 MHz with 4.7 kΩ pullup)

Because of my microprocessor I2C eratta problems I need to develop a "bit bashed" I2C for the FIFO transfer.

This is why I am interested in the max clock speed I can achieve.

best regards johnc

0 Kudos
Reply

1,230 Views
david_diaz
NXP Employee
NXP Employee

Hello John,

My apologies for the delay.

Definitely, this is an error in the datasheet. Please rely on the specifications mentioned on table 4 from the datasheet and not on the features section in front page.

I hope this information helps.

Regards,

David

0 Kudos
Reply

1,230 Views
johncampbell
Contributor II

David,

Thanks.

I will adjust my speed to the maximum allowed by the timing in the table 4. (with some margin of course)

Regards johnc

0 Kudos
Reply