MMA68XX initialization

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MMA68XX initialization

1,050 次查看
shimasaadat
Contributor I

Hi,

I’m new at working with MMA68xx. I work on a reverse engineering project and read the micro commands and sensor responses through a SPI interface on the other test board. The initial state commands and responses are as below:

16 Clock cycles

commands

responses

1st

0X4A00

0X0E00

2nd

0X4AC0

0X3E00

3rd

0XCA40

0X3E00

  Every command is sent in 16 -clock cycles and its response come from sensor in the next 16 clock cycles.

The first command is sent in the first 16 clock cycles according to the SPI interface the response message in this step must be 0X0000 but in first clock cycle I have a response which says Invalid register address….

Another question:

These 3 commands reset the device but to terminate the reset a read of DEVCTL register is needed (It is written in datasheet), but after these commands I can’t find this command…

标签 (1)
标记 (1)
0 项奖励
1 回复

743 次查看
reyes
NXP TechSupport
NXP TechSupport

Hi shima saadat,

Here is another thread from the Freescale Communities which might give you some clues.

It talks about configuring the MMA68xx.

MMA68xx initialization

And as mentioned in the communities thread: Information (hardware and source code) is available at Automotive Sensors Tower System Module Freescale

Refer driver for MMA6800.


Have a great day,
Jose Reyes

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励