MAG3110 reliability under strong magnetic flux

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MAG3110 reliability under strong magnetic flux

ソリューションへジャンプ
1,510件の閲覧回数
ble
Contributor I

Hello,

I am developing a device with MAG3110 magnetometer. It will be used in an area with strong magnetic flux.

I wondered whether it will shorten the life of the MAG3110 or should I expect it to work fine for the normal life of the MAG3110? (Which is how long?)

Thanks

タグ(1)
0 件の賞賛
1 解決策
1,235件の閲覧回数
Joshevelle
Senior Contributor I

Hello Ariel,

The sensor would not be damaged as long as you don't exceed the maximum magnetic field it can support (100,000uT). Since the life spam of the device would depend on the customer application, we do not have an estimate of life.

I highly recommend you to take a look at the following application note, which describes how to calibrate the MAG3110 in the presence of hard and soft iron interference:

http://cache.freescale.com/files/sensors/doc/app_note/AN4246.pdf

Hope it helps!

Josh

元の投稿で解決策を見る

0 件の賞賛
1 返信
1,236件の閲覧回数
Joshevelle
Senior Contributor I

Hello Ariel,

The sensor would not be damaged as long as you don't exceed the maximum magnetic field it can support (100,000uT). Since the life spam of the device would depend on the customer application, we do not have an estimate of life.

I highly recommend you to take a look at the following application note, which describes how to calibrate the MAG3110 in the presence of hard and soft iron interference:

http://cache.freescale.com/files/sensors/doc/app_note/AN4246.pdf

Hope it helps!

Josh

0 件の賞賛