s32k146 evb: can't probe with opensda

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

s32k146 evb: can't probe with opensda

跳至解决方案
853 次查看
frank-li2021
Contributor III

之前在 kw36 evb 碰到过同样的问题,不能使用 opensda 进行 debug,更新 opensda 固件,变成 jlink 即可。

so 我的问题在哪里可以下载到 opensda 的固件更新为 jlink 设备

0 项奖励
回复
1 解答
845 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi Frank,

Please download the V1 J-Link OpenSDA - Generic Firmwares.
Try to solve the OpenSDA connection problem refer: s32k144 is not working debug by opensda in s32k144 EVB

J-Link OpenSDA - Generic Firmwares.png

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

在原帖中查看解决方案

1 回复
846 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi Frank,

Please download the V1 J-Link OpenSDA - Generic Firmwares.
Try to solve the OpenSDA connection problem refer: s32k144 is not working debug by opensda in s32k144 EVB

J-Link OpenSDA - Generic Firmwares.png

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------