there are no some module in RTDs
I have installed RTD 4.0.0 P16 and 4.0.0 P20, but there is no fls and fee moudes in the EB config page when i choose ASAR4.7 version
but when i choose ASAR 4.4, the version of other modules is V2.0.0, which are not the modules in this RTD
so, i can not use the RTD to create a project with RTD version v4.0.0
Hi
This is the Significant Change between AUTOSAR 4.4 and 4.7:
Please use those new modules when using AUTOSAR 4.7 version.
Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Thanks for your kind reply. I must appologyze for the statements of my question.
my question is that
when i choose ASAR4.4, the version of fls and fee is V4.0.0, but the version of other modules,such as canif, adc is not V4.0.0,so I can not create a ASAR4.4 project with all needed modules that with version 4.0.0
Unfortunately, all S32K3 v4.0.0 releases only support ASR R21-11 in whole or in part (ASR 4.4 is supported on Memory drivers in a few releases).
That means there won't be a release package that matches your requirements. Even older release package - v3.0.0 has started supporting ASR R21-11 instead of ASR 4.4.
So I think you should use v4.0.0 P20 with a mixed configuration between ASR R21-11 and ASR 4.4.
canif, adc... are not of S32K3_S32M27x Real-Time Drivers ASR 4.4 Version 4.0.0 P20. I guess you have installed more than S32K3 P16 and S32K3 P20.
Look on the Release Notes of P20:
So, it means P20 provide Fee, Fls, Eep on asr 4.4.0 and the rest on asr 21-11