Currently, I use S32K144 and Our Project must run from SRAM to do a partition of memory.
I try to download new firmware on SRAM using JFlash tool.
But I can't do this.
Could you please help me with this issue?
BRs
Hyunung Park
Solved! Go to Solution.
Hi, I have a similar requirement, and being new to NXP products I am still learning. Is the only way to do this procedure (flash to SRAM for memory partition) with a JFLash? or can I do it by dragging the .mot file into the board (i.e. using a direct PC to board connection through micro USB) I also have a PE micro multilink adaptor. Best regards.
Hi, I have a similar requirement, and being new to NXP products I am still learning. Is the only way to do this procedure (flash to SRAM for memory partition) with a JFLash? or can I do it by dragging the .mot file into the board (i.e. using a direct PC to board connection through micro USB) I also have a PE micro multilink adaptor. Best regards.
Hi @whinojo,
If you have a project in S32DS IDE, set the Build configuration to Debug_RAM and compile it.
Right-click on the project in Project Explorer
In Debug Configuration, you can choose either Segger J-link or PE Micro and load it to the MCU.
BR, Daniel
Hello Hyunung Park,
I would recommend contacting Segger support.
JFlash is not an NXP product.
BR, Daniel