Hello Nxp Team,
We are using S32K148 controller in our project.
We have to read the speed information by configuring the FTM module.
controller is manipulating the speed information in terms of pulses.
controller has to read the pulses received through FTM channel.
I used some Example code of S32k148 (input capture code), but I can not find the pulses count without interrupt configuration.
We can find the frequency and time of the one pulse.
I did not understand the some part of the FTM module in Reference manual.
could you please help me with name the hardware register to read the input pulse count value.
I don't want to configure interrupt(executing ISR for every pulse) for Input capture example, it will waste CPU time.
controller may read more than 2000 pulses per second .
Kindly help me, Thanks in advance.
Regards,
Ambarish
Hello Ambarish,
The FTM counter clock can be clocked by external clocks from TCLK pins. So, there is a possible route the timer to the TCLK pin.
Or you can use the PTC29 as GPIO and generate an interrupt on the rising edge.
I hope it helps you.
Best Regards,
Diana
Hi,
Please check Quadrature Decoder – Count and Direction Encoding mode.
In this mode the FTM driver will be driven by your sensor output. The disadvantage is you must use also phase B pin to control counting direction.
If you must use only one pin for your application you can switch to LPTMR module which provides pulse counter feature.
In SDK you can find example for LPTMR pulse counter.
Best regards,
Razvan
Hello,
Thank you.
do not want check the direction , need to count only pulses(it is for tachy update).
Could you please share me the example code for the pulse counting(FTM channel code).
Yes, we can measure the pulse by LPTMR, but Our hardware(FTM pin is used in Hardware) is using the FTM for pulse counting.
Thank you in advance.
Regards,
Ambarish
Hi,
I can develop the example, but you can configure only these pins for quadrature decoder:
Also, is mandatory to use both signals (direction and input signal), so in your case you must connect phase b to high, or to leave it floating with pull up enabled (I'm not sure if the second solution works).
Let me know which FTM pins are used in your application.
Best regards,
Razvan
Hi,
In this case you must re-work your hardware :smileysad:. With that pin is impossible to implement the solutions proposed by me and by dianabatrlova.
With this hardware you have just to count the edges in software by interrupt handler, but as you already observed the CPU load can be high.
Best regards,
Razvan