Why is the data received by LPSPI from the slave out of order?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Why is the data received by LPSPI from the slave out of order?

1,581 Views
kalvin
Contributor I

One of the two MCUs is the master and the other is the slave. The master starts DMA sending/receiving every 5ms and triggers the slave to start DMA receiving/sending through the external interrupt signal (IND).

void MainFunctionRun(void)
{
if(!Task_Delay[0])
{
Task_Delay[0] = 5; //loop every 5ms

SpiMaster_EmitInd(PTE,IND);

DMA_Start(SPI_DMA_RX_CH,SPI_DMA_TX_CH); //master start DMA for spi
}
}

void PORTE_IRQHandler(void)
{
if(((PTE->PDIR >> IND) & 1) == 0) //slave received IND signal
{
DMA_Start(SPI_DMA_RX_CH,SPI_DMA_TX_CH); //slave start DMA for spi
}
else if(((PTE->PDIR >> ACK) & 1) == 0) //no use
{
}
PORTE->ISFR |= (1<<IND)|(1<<ACK);
}

0 Kudos
Reply
5 Replies

1,556 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

Such effect are usually caused by overflow/underflow condition. How you are triggering DMA transfer on the slave side?

0 Kudos
Reply

1,540 Views
kalvin
Contributor I

In the above code fragment PORTE_IRQHandler, before the master DMA starts, the IND signal will be sent to the slave to trigger the slave DMA reception.

0 Kudos
Reply

1,520 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

It is unusual approach. It is needed to route DMA request directly from LPSPI to DMA module (with using of DMAMUX)

davidtosenovjan_0-1664786751929.png

 

0 Kudos
Reply

1,465 Views
kalvin
Contributor I

@davidtosenovjan any new answers ?

0 Kudos
Reply

1,502 Views
kalvin
Contributor I

I also used DMAMUX @davidtosenovjan .

static void DMAMUX_Init(LPSPI_Type *Instance,uint8_t rxch,uint8_t txch)
{
uint32_t DMA_CH_RX_MUX_NUM = 0; 
if(Instance == LPSPI0) DMA_CH_RX_MUX_NUM = 14;                                //using LPSPI0
if(Instance == LPSPI1) DMA_CH_RX_MUX_NUM = 16;
if(Instance == LPSPI2) DMA_CH_RX_MUX_NUM = 18;

SIM->PLATCGC |= SIM_PLATCGC_CGCDMA(1); 
PCC->PCCn[PCC_DMAMUX_INDEX] |= PCC_PCCn_CGC_MASK; 

/* DMA Channel 4 for LPSPI RX */
DMAMUX->CHCFG[rxch] &= ~ DMAMUX_CHCFG_ENBL(1); 
DMAMUX->CHCFG[rxch] |= DMAMUX_CHCFG_SOURCE(DMA_CH_RX_MUX_NUM); //14
DMAMUX->CHCFG[rxch] |= DMAMUX_CHCFG_ENBL(1); 
/* DMA Channel 5 for LPSPI TX */
DMAMUX->CHCFG[txch] &= ~ DMAMUX_CHCFG_ENBL(1); 
DMAMUX->CHCFG[txch] |= DMAMUX_CHCFG_SOURCE(DMA_CH_RX_MUX_NUM+1); //14+1
DMAMUX->CHCFG[txch] |= DMAMUX_CHCFG_ENBL(1); 
}

0 Kudos
Reply