Trigger more than 8 ADC channels with PDB

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Trigger more than 8 ADC channels with PDB

跳至解决方案
2,715 次查看
mrsmml
Contributor I

Hi,

I want to trigger more than 8 ADC conversions of ADC module 1 with the PDB1 module with only one software trigger (PDB_DRV_SoftTriggerCmd). I can only get to work either the first 8 ADC channels (with PDB1 CH0) or the remaining "x" ADC channels with (PDB1 CH1).

Is it possible to trigger all 13 ADC conversions of both PDB1 channels with only one trigger.

Here is the current configuration.

   

   // PDB 1 init and setup
    PDB_DRV_Init(INST_PDB2, &pdb1_InitConfig0);
    PDB_DRV_ConfigAdcPreTrigger(INST_PDB2, 0UL, &pdb2_AdcTrigInitConfig0);  // for ADC1 channel 0
    PDB_DRV_ConfigAdcPreTrigger(INST_PDB2, 0UL, &pdb2_AdcTrigInitConfig1);  // for ADC1 channel 1
    PDB_DRV_ConfigAdcPreTrigger(INST_PDB2, 0UL, &pdb2_AdcTrigInitConfig2);  // for ADC1 channel 2
    PDB_DRV_ConfigAdcPreTrigger(INST_PDB2, 0UL, &pdb2_AdcTrigInitConfig3);  // for ADC1 channel 3
    PDB_DRV_ConfigAdcPreTrigger(INST_PDB2, 0UL, &pdb2_AdcTrigInitConfig4);  // for ADC1 channel 4
    PDB_DRV_ConfigAdcPreTrigger(INST_PDB2, 0UL, &pdb2_AdcTrigInitConfig5);  // for ADC1 channel 5
    PDB_DRV_ConfigAdcPreTrigger(INST_PDB2, 0UL, &pdb2_AdcTrigInitConfig6);  // for ADC1 channel 6
    PDB_DRV_ConfigAdcPreTrigger(INST_PDB2, 0UL, &pdb2_AdcTrigInitConfig7);  // for ADC1 channel 7

    PDB_DRV_ConfigAdcPreTrigger(INST_PDB2, 1UL, &pdb2_AdcTrigInitConfig8);  // for ADC1 channel 8
    PDB_DRV_ConfigAdcPreTrigger(INST_PDB2, 1UL, &pdb2_AdcTrigInitConfig9);  // for ADC1 channel 9
    PDB_DRV_ConfigAdcPreTrigger(INST_PDB2, 1UL, &pdb2_AdcTrigInitConfig10); // for ADC1 channel 10
    PDB_DRV_ConfigAdcPreTrigger(INST_PDB2, 1UL, &pdb2_AdcTrigInitConfig11); // for ADC1 channel 11
    PDB_DRV_ConfigAdcPreTrigger(INST_PDB2, 1UL, &pdb2_AdcTrigInitConfig12); // for ADC1 channel 12
    PDB_DRV_ConfigAdcPreTrigger(INST_PDB2, 1UL, &pdb2_AdcTrigInitConfig13); // for ADC1 channel 13

    PDB_DRV_SetTimerModulusValue(INST_PDB2, (uint32_t)delayValue);
    PDB_DRV_SetAdcPreTriggerDelayValue(INST_PDB2, 0UL, 0UL, (uint32_t)delayValue);
    PDB_DRV_SetAdcPreTriggerDelayValue(INST_PDB2, 1UL, 0UL, (uint32_t)delayValue);
    PDB_DRV_LoadValuesCmd(INST_PDB2);
    PDB_DRV_SoftTriggerCmd(INST_PDB2);

// PDB config

const pdb_timer_config_t pdb1_InitConfig = {
  .loadValueMode = PDB_LOAD_VAL_IMMEDIATELY,
  .seqErrIntEnable = false,
  .clkPreDiv = PDB_CLK_PREDIV_BY_2,
  .clkPreMultFactor = PDB_CLK_PREMULT_FACT_AS_10,
  .triggerInput = PDB_SOFTWARE_TRIGGER,
  .continuousModeEnable = false,
  .dmaEnable = false,
  .intEnable = false,
};

const pdb_adc_pretrigger_config_t pdb2_AdcTrigInitConfig0 = {
  .adcPreTriggerIdx = 0U,
  .preTriggerEnable = true,
  .preTriggerOutputEnable = true,
  .preTriggerBackToBackEnable = false,
};

const pdb_adc_pretrigger_config_t pdb2_AdcTrigInitConfig1 = {
  .adcPreTriggerIdx = 1U,
  .preTriggerEnable = true,
  .preTriggerOutputEnable = true,
  .preTriggerBackToBackEnable = true,
};

const pdb_adc_pretrigger_config_t pdb2_AdcTrigInitConfig2 = {
  .adcPreTriggerIdx = 2U,
  .preTriggerEnable = true,
  .preTriggerOutputEnable = true,
  .preTriggerBackToBackEnable = true,
};

const pdb_adc_pretrigger_config_t pdb2_AdcTrigInitConfig3 = {
  .adcPreTriggerIdx = 3U,
  .preTriggerEnable = true,
  .preTriggerOutputEnable = true,
  .preTriggerBackToBackEnable = true,
};

const pdb_adc_pretrigger_config_t pdb2_AdcTrigInitConfig4 = {
  .adcPreTriggerIdx = 4U,
  .preTriggerEnable = true,
  .preTriggerOutputEnable = true,
  .preTriggerBackToBackEnable = true,
};

const pdb_adc_pretrigger_config_t pdb2_AdcTrigInitConfig5 = {
  .adcPreTriggerIdx = 5U,
  .preTriggerEnable = true,
  .preTriggerOutputEnable = true,
  .preTriggerBackToBackEnable = true,
};

const pdb_adc_pretrigger_config_t pdb2_AdcTrigInitConfig6 = {
  .adcPreTriggerIdx = 6U,
  .preTriggerEnable = true,
  .preTriggerOutputEnable = true,
  .preTriggerBackToBackEnable = true,
};

const pdb_adc_pretrigger_config_t pdb2_AdcTrigInitConfig7 = {
  .adcPreTriggerIdx = 7U,
  .preTriggerEnable = true,
  .preTriggerOutputEnable = true,
  .preTriggerBackToBackEnable = true,
};

const pdb_adc_pretrigger_config_t pdb2_AdcTrigInitConfig8 = {
  .adcPreTriggerIdx = 0U,
  .preTriggerEnable = true,
  .preTriggerOutputEnable = true,
  .preTriggerBackToBackEnable = true,
};

const pdb_adc_pretrigger_config_t pdb2_AdcTrigInitConfig9 = {
  .adcPreTriggerIdx = 1U,
  .preTriggerEnable = true,
  .preTriggerOutputEnable = true,
  .preTriggerBackToBackEnable = false,
};

const pdb_adc_pretrigger_config_t pdb2_AdcTrigInitConfig10 = {
  .adcPreTriggerIdx = 2U,
  .preTriggerEnable = true,
  .preTriggerOutputEnable = true,
  .preTriggerBackToBackEnable = true,
};

const pdb_adc_pretrigger_config_t pdb2_AdcTrigInitConfig11 = {
  .adcPreTriggerIdx = 3U,
  .preTriggerEnable = true,
  .preTriggerOutputEnable = true,
  .preTriggerBackToBackEnable = true,
};

const pdb_adc_pretrigger_config_t pdb2_AdcTrigInitConfig12 = {
  .adcPreTriggerIdx = 4U,
  .preTriggerEnable = true,
  .preTriggerOutputEnable = true,
  .preTriggerBackToBackEnable = true,
};

const pdb_adc_pretrigger_config_t pdb2_AdcTrigInitConfig13 = {
  .adcPreTriggerIdx = 5U,
  .preTriggerEnable = true,
  .preTriggerOutputEnable = true,
  .preTriggerBackToBackEnable = true,
};

Regards

Marius

0 项奖励
回复
1 解答
2,268 次查看
martinhoffmann2
Contributor II

Yes!

But the first entry of PDB Channel 1 has to have an explicit trigger time (no back-to-back possible for the first entry, the remaining 7 entries of the channel 1 list can be set to back-to-back again).

Take care: The first trigger time of channel 1 has to be after the last measurement of PDB channel 0.

BR

Martin

在原帖中查看解决方案

0 项奖励
回复
4 回复数
2,268 次查看
danielmartynek
NXP TechSupport
NXP TechSupport

Hi Marius,

This is not possible, but you can chain PDB0 CH0 and PDB1 CH0 when SIM_CHIPCTL[PDB_BB_SEL] = 1.
Please see Figure 44-3 and Figure 44-4 in the RM rev.9.

Regards,
Daniel

0 项奖励
回复
2,268 次查看
mrsmml
Contributor I

Hi Daniel,

thank you for your reply. In this case, I would like to re-phrase my question.

How is it possible to trigger more than 8 ADC channels of one ADC module using one PDB module (with channel 0 and 1) using software trigger and back-to-back mode.

Regards,

Marius

0 项奖励
回复
2,269 次查看
martinhoffmann2
Contributor II

Yes!

But the first entry of PDB Channel 1 has to have an explicit trigger time (no back-to-back possible for the first entry, the remaining 7 entries of the channel 1 list can be set to back-to-back again).

Take care: The first trigger time of channel 1 has to be after the last measurement of PDB channel 0.

BR

Martin

0 项奖励
回复
2,267 次查看
liuweiliang
Contributor II

I have the same needs.
I tried to change the trigger time as you said. When the trigger time is changed to 4000, only ADC1->RA to ADC1->RH have data. When the trigger time is changed to 3500, there is no data in ADC1->RA to ADC1->RH, and ADC1->RI has data.
I don't know where the problem is, can you help me see it?

0 项奖励
回复