The issue of the FLS module not being included in S32K3 RTD 4.0.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

The issue of the FLS module not being included in S32K3 RTD 4.0.

182 次查看
gumu
Contributor IV

Dear Sir,

Recently, when I was using RTD 4.0, I found that the FLS module was not available for selection in a new project. The version I installed is: SW32K3_S32M27x_RTD_R21-11_4.0.0_D2311_DS_updatesite.zip. Screenshot below:

gumu_0-1716788399718.png

Is it possible that the FLS module in the new version of RTD has been replaced by INFLS and EXFLS modules?

Thanks!

标记 (1)
0 项奖励
回复
1 回复

161 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

Because this RTD is based on AUTOSAR R21-11, there is no FLS module.

Please refer to the discussion in no fee and fls modules in RTD of s32k3x


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复