S32k project no sdk source?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32k project no sdk source?

Jump to solution
914 Views
jinsheng20
Contributor III

hello:

    ploatform:s32ds win32 2.2  hardware:s32k116

  I created the project with HelloWorld Demo, but there is no source file in the SDK directory under the project directory?How do I configure to see the SDK source code in the project directory?

 

0 Kudos
Reply
1 Solution
907 Views
PetrS
NXP TechSupport
NXP TechSupport
0 Kudos
Reply
2 Replies
908 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

 

modify a ProcessorExpert.pe file as suggested e.g. in https://community.nxp.com/t5/S32-Design-Studio/s32k-example-project-accessing-files-on-system-direct...

 

BR, Petr

0 Kudos
Reply
913 Views
jinsheng20
Contributor III

15.png

0 Kudos
Reply