S32K322NHT0MPAST GPIO Pin's Max and Min current for input and output.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K322NHT0MPAST GPIO Pin's Max and Min current for input and output.

87 Views
Chinnan
Contributor II

Hi Sir,

 

Could you please share what is the  S32K322NHT0MPAST  GPIO pin's max and minimum Sink and source current?

 

 

Regards,

CHINNAN 

0 Kudos
1 Reply

66 Views
Julián_AragónM
NXP TechSupport
NXP TechSupport

Hi @Chinnan,

Please refer to S32K3xx Data Sheet's Table 7 I/O parameters, where you can find input leakage current and output high current for GPIO.

The higher the current the bigger the voltage drop from VDD/VSS. The datasheet specifies the min. guaranteed current at  

VOL <= 0.7V

VOH >= VDD_HV_A/B - 0.7V

for all the GPIO types.

Best regards,
Julián

0 Kudos