Hi. I tried to use STM0 module in EB tresos studio.
SW: S32DSIDE 3.5 RTD4.0.0 P04, S32K312
problem:
I config EB according to GPT samples. use continous mode. When debugging, the code is blocked at GPT_Init when call Stm_Ip_SetDebugMode. PIT0_CH0 works normal.
see snapshots.
Also I tried to config STM0 in S32DSIDE+RTDSDK. Gpt_Init is not blocked. but Its notification trigger is not normal. when triggered 2 times, next trigger will wait a long time.
the attachment is the project configured in IDE。
Can some provide a sample STM0 config in EBtresOS?