S32K3 GPIO DC electrical specifications

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K3 GPIO DC electrical specifications

Jump to solution
309 Views
Chinnan
Contributor II

 

When i applied an varying voltage from 0 to 3.3V to controller Pin, The microcontroller taking 1.65 as Input high. Also when i decrease high to low (Ie, 3.3V to 0V) at 1.58V microcontroller took as Input Low.

As per data sheet, For 3.3V microcontroller Input high voltage is 0.7 VDD to VDD and Input low is 0V to 0.3 VDD.

 

1, Why microcontroller taking 1.65 as Input high? Any software setting required to change or not?

2, What will actually happen in between an voltage comes VIL and VIH?

3, What is the transition voltage of microcontroller?

0 Kudos
Reply
1 Solution
293 Views
Julián_AragónM
NXP TechSupport
NXP TechSupport

Hi @Chinnan,

You can find inside the following document, section "Input Characteristics": AN2434: Input/Output Pin Drivers on HCS12 Family MCUs, which still applies to S32K3 family:

Julin_AragnM_0-1715708563505.png

When defining VIH or VIL, it is generally set at 70% or 30% of VDD so it is guaranteed that the input reads either LOW or HIGH when input passes those thresholds levels.

Many factors affect the transition voltage level for the MCU, such as temperature. That is why a specific transition voltage is not specified, it is not possible to predict which logic level the MCU will interpret.

Best regards,
Julián

View solution in original post

4 Replies
294 Views
Julián_AragónM
NXP TechSupport
NXP TechSupport

Hi @Chinnan,

You can find inside the following document, section "Input Characteristics": AN2434: Input/Output Pin Drivers on HCS12 Family MCUs, which still applies to S32K3 family:

Julin_AragnM_0-1715708563505.png

When defining VIH or VIL, it is generally set at 70% or 30% of VDD so it is guaranteed that the input reads either LOW or HIGH when input passes those thresholds levels.

Many factors affect the transition voltage level for the MCU, such as temperature. That is why a specific transition voltage is not specified, it is not possible to predict which logic level the MCU will interpret.

Best regards,
Julián

278 Views
Chinnan
Contributor II

Is there any way in the software that any input voltage between 0.3VDD to 0.65VDD on the GPIO pin can be taken as low or high?

0 Kudos
Reply
262 Views
Julián_AragónM
NXP TechSupport
NXP TechSupport

Hi @Chinnan,

You could set your desired voltage input as a reference by configuring an ADC and using that value as a low or high.

Best regards,
Julián

0 Kudos
Reply
307 Views
Chinnan
Contributor II

The Microcontroller was S32K322NHT0MPAST  100 Pin HDQFP

0 Kudos
Reply