S32K1xx Interrupt Wake-up from other location than main.c

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32K1xx Interrupt Wake-up from other location than main.c

ソリューションへジャンプ
1,088件の閲覧回数
ndousse
Contributor II

Hello,

I am trying to implement a sleep wake-up procedure on the S32K146 development board. 

To send the controller to sleep, I use the code from the Application notes AN5425, chapter 5.5.1. 

S32_SCB->SCR |= S32_SCB_SCR_SLEEPDEEP(1);
/* Select Stop Mode */
SMC->PMCTRL = SMC_PMCTRL_STOPM(0b00);
/* Select which STOP mode (Stop1 or Stop2)
 * is desired (Stop1 - 0b01, Stop2 - 0b10) */
SMC->STOPCTRL = SMC_STOPCTRL_STOPO(0b01);
/* Wait For Interrupt */
#if defined (__GNUC__)
__asm volatile ("wfi");
#endif

The go to sleep procedure works without any issue, no matter the stop mode that I use. 

To wake-up the controller, I want to trigger a LIN interruption using the LIN 2.1 stack from the NXP SDK. LIN communication is working properly. 

 

Issue that I am facing:

  • If the command "__asm volatile ("wfi");" is called from the file "main.c", the wake-up procedure through LIN (or a pin interruption based on a button pressed on the development board) works without any issue.
  • However, if I moved this command to another file, I cannot trigger any interruption to wake-up the controller (neither a LIN interruption nor a Pin based interruption based on the button of the development board). 
  • I also tried to use the NXP SDK power manager module generated from the Processor Expert and face exactly the same issue. 

My question:

What do I need to define or modify in order to be able to wake-up the controller from any file?

Thank you for your guidance.

0 件の賞賛
1 解決策
1,057件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hello @ndousse,

The MCU starts running in the wakeup ISR, and once the ISR is complete, it returns to the next inxtruction after WFI.

So, if the AWIC does not detect the interrupt, please make sure that when the WFI is executed

  • the interrupts are not masked
  • the WFI is not in an ISR that cannot be preempted (higher priority).

 

Regards,

Daniel

元の投稿で解決策を見る

0 件の賞賛
4 返答(返信)
1,043件の閲覧回数
ndousse
Contributor II

Dear Daniel,

Thank you for your answer. 

The "__asm volatile ("wfi");" is indeed called from an interrupt, a scheduler based on a lptmr interrupt. The LPTMR_DRV_ClearCompareFlag is cleared directly at the beginning of the interrupt, before the call to the "wfi". 

No interrupt mask is applied. 

All the interruption have their default priority. Following the S32K1xx_DMA_Interrupt_mapping.xlsx, the LPUART interrupts have a lower Interrupt ID (ID 31-35) than the LPTMR interrupt ID (ID 58). So the LPUART should have a higher priority than the LPTMR, is it correct?

Can I simply change the priority of the LPTMR interrupt to a lower one in order to trigger the LPUART interrupt as AWIC?

0 件の賞賛
1,039件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @ndousse,

If all the interrupts have thier priority set to 0 (default), one interrupt can't preempt the other.

You would need to set the LPTMR interrupt to a lower periority (like 1).

 

BR, Daniel

0 件の賞賛
1,028件の閲覧回数
ndousse
Contributor II

Dear Daniel,

I setup the priority of the LPTMR interruption to 1 with the function

 

INT_SYS_SetPriority(LPTMR0_IRQn, 1);

 

And I was able to trigger the LIN interruption through LPUART. 

Thanks for your guidance and help.

1,058件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hello @ndousse,

The MCU starts running in the wakeup ISR, and once the ISR is complete, it returns to the next inxtruction after WFI.

So, if the AWIC does not detect the interrupt, please make sure that when the WFI is executed

  • the interrupts are not masked
  • the WFI is not in an ISR that cannot be preempted (higher priority).

 

Regards,

Daniel

0 件の賞賛