S32K148 - SAI TX overflows

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K148 - SAI TX overflows

1,080 Views
jakub_mielczare
Contributor III

Hello,

Is there any way to check if there are overflows on SAI0 TX FIFOs when DMA is feeding SAI?

The S32K148 Reference Manual specifies how to check if there was underrun, but I could not find similar interrupt for overflow. I would need this information as soon as overflow happens.

Thank you,

Jakub

Tags (1)
0 Kudos
Reply
7 Replies

928 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

TX FIFO can underrun, RX FIFO can overflow. But TX FIFO can't overflow and RX FIFO can't underrun.

If DMA is used for TX FIFO and there's no empty space in the FIFO, the DMA request is simply not asserted. It's asserted only when the FIFO is not full.

Regards,

Lukas

0 Kudos
Reply

928 Views
jakub_mielczare
Contributor III

Hi Lukas,

Can TX FIFO overflow, when e.g. watermark is set to 1 and DMA transfer is set to 2x 4samples (each sample is 32-bit).

In this case DMA request would be generated by SAI when there is 1 word left in FIFO? Can DMA write 8 words before the last 1 sample leaves FIFO?

Thanks,

Jakub

0 Kudos
Reply

928 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

pastedImage_1.png

It means you have to configure the DMA in a way that it cannot happen.

Regards,

Lukas

0 Kudos
Reply

928 Views
jakub_mielczare
Contributor III

Hi,

Is there any way to diagnose, that such condition has happened, i.e. transmit FIFO write was ignored, because the FIFO was full?

Regards,

Jakub

0 Kudos
Reply

928 Views
jakub_mielczare
Contributor III

Hello,

Is there any update for this thread?

Regards,

Jakub

0 Kudos
Reply

928 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi Jakub,

sorry, I somehow missed that question.

No, it's simply ignored. It's user responsibility to ensure that full FIFO is not written. If DMA is not used, it's necessary to confirm before each write that FIFO is not full. If DMA is used then DMA descriptor must be configured in a way that only one sample is written to FIFO per one HW request. Then it is ensured that full FIFO will not be written again because there will be no HW trigger in this case.

In other words, it's necessary to avoid this situation, not to handle the consequences.

Regards,

Lukas

0 Kudos
Reply

928 Views
jakub_mielczare
Contributor III

Hi Lukas,

Thank you for the answer.

Regards,

Jakub

0 Kudos
Reply