S32K118的pflash和dflash如何使用

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K118的pflash和dflash如何使用

Jump to solution
225 Views
Vapaus
Contributor III

S32K118的pflash和dflash如何配置并且使用

0 Kudos
Reply
1 Solution
198 Views
Julián_AragónM
NXP TechSupport
NXP TechSupport

Hi @Vapaus

You can find some flash examples inside the Real-Time Drivers (RTD) package.

Julin_AragnM_0-1717533601671.png

To install this RTD version you need to download the UpdateSite.zip file from the flexera portal. Once you have it, at S32DS Extensions and Updates, click "Add Update Site" and select the zip file, then click Open, you need to select the file and then Install.

Best regards,
Julián

View solution in original post

0 Kudos
Reply
1 Reply
199 Views
Julián_AragónM
NXP TechSupport
NXP TechSupport

Hi @Vapaus

You can find some flash examples inside the Real-Time Drivers (RTD) package.

Julin_AragnM_0-1717533601671.png

To install this RTD version you need to download the UpdateSite.zip file from the flexera portal. Once you have it, at S32DS Extensions and Updates, click "Add Update Site" and select the zip file, then click Open, you need to select the file and then Install.

Best regards,
Julián

0 Kudos
Reply