S32K118的pflash和dflash如何使用

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32K118的pflash和dflash如何使用

ソリューションへジャンプ
292件の閲覧回数
Vapaus
Contributor III

S32K118的pflash和dflash如何配置并且使用

0 件の賞賛
返信
1 解決策
265件の閲覧回数
Julián_AragónM
NXP TechSupport
NXP TechSupport

Hi @Vapaus

You can find some flash examples inside the Real-Time Drivers (RTD) package.

Julin_AragnM_0-1717533601671.png

To install this RTD version you need to download the UpdateSite.zip file from the flexera portal. Once you have it, at S32DS Extensions and Updates, click "Add Update Site" and select the zip file, then click Open, you need to select the file and then Install.

Best regards,
Julián

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
266件の閲覧回数
Julián_AragónM
NXP TechSupport
NXP TechSupport

Hi @Vapaus

You can find some flash examples inside the Real-Time Drivers (RTD) package.

Julin_AragnM_0-1717533601671.png

To install this RTD version you need to download the UpdateSite.zip file from the flexera portal. Once you have it, at S32DS Extensions and Updates, click "Add Update Site" and select the zip file, then click Open, you need to select the file and then Install.

Best regards,
Julián

0 件の賞賛
返信