S32K116 is locked while Flash Erase using CSEC. How to unlock it? Is there any tool?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32K116 is locked while Flash Erase using CSEC. How to unlock it? Is there any tool?

2,686件の閲覧回数
muhammetkalayci
Contributor II

Hello,

my MCU is locked while flash erasing due to secured flash memory in CSEC operations.

I found out the problem but now I want to unlock my MCU. 

 

Is there any way unlocking it? hard resetting? maybe NXP has a tool for that?

(I cannot connect not debugging, nor j-flash)

I am open to any solution.

0 件の賞賛
返信
3 返答(返信)

2,630件の閲覧回数
muhammetkalayci
Contributor II

Hello, 

I have tried both of them. In the first one, there was a power connection issue. 

As a result, they did not solve the issue.

 

@Senlent Now, I want to ask if there is not any way to unlock mcu; I need a clear guide for erasing flash that will not lock again any chance.

Because this is 3rd mcu that is locked and I dont have much in backup. 

Please provide me a clear and solid guideline. 

 

Thank you,

Sincerely.

0 件の賞賛
返信

2,624件の閲覧回数
Senlent
NXP TechSupport
NXP TechSupport

Hi@muhammetkalayci

you can take a look at the AN12130,

https://www.nxp.com/docs/en/application-note/AN12130.pdf 

The chapter:3.2.5.2 Mass erase and CSEc considerations 

 

In order for you to better understand these modules, you can also take a look at the following two documents

Using the Kinetis Security and Flash Protection Features 

Getting Started with CSEc Security Module 

 

These are some application notes I could find, maybe they can help you

 

0 件の賞賛
返信

2,670件の閲覧回数
Senlent
NXP TechSupport
NXP TechSupport

Hi@muhammetkalayci

1.please try to use J-LINK to read the register of MDM_AP 

for example:

Senlent_0-1675763344079.png

According to AN4507 :https://www.nxp.com/search?keyword=AN4507&start=0 

"If  the user disables mass erase with no other means to unsecure the device (no backdoor key and no firmware means of changing the default security options), then that device will be permanently secured."

 

2.If your J-Link can not connect to MCU, you can have a try to use the software provided in the below link.

Bricking and Recovering FRDM-KL25Z Boards: Reset, SWD Clock and Low Power

https://mcuoneclipse.com/2013/06/16/bricking-and-recovering-frdm-kl25z-boards-reset-swd-clock-and-lo... 

 

 

0 件の賞賛
返信