to reuse the buffer and reduce the ram, I do not wanna to use more than two channels in a job.
I wanna to reuse the channel to reissue a spi communication in the SpiSeqEndNotification callback
the details is shown below
after i handle the data in the SpiSeqEndNotification callback ,i reissue a new seq but no response.
the MCU is S32K344
the RTD is RTD 2.0.0
Hello @LewisThin,
I'm not sure I understand.
Can you elaborate? Can you share the project?
Do you use two LPSPI instances, one as a master and one as a slave?
Do you measure the bus with an oscilloscope?
Regards,
Daniel