Just to be sure, to run the example you will need to have the following items:
Be sure to have this before running the project.
B.R.
VaneB
Hi @VaneB
All the configurations are done in the same way as the master. The code is flashed successfully in the Board but it's not responding to the master header and not receiving the response sent by the master.
Regards,
Bhavesh Raju
The guide on how to run the example you can find it located at C:\nxp\S32DS_ARM_v2.2\S32DS\software\S32SDK_S32K1xx_RTM_3.0.0\doc\Start_here.html -> S32K148 -> Examples and Demos -> Demo Applications.
This is just an example but is almost the same for S32DS v3.4 and 3.5.
Hi @VaneB
I generated the processor code with 176 pins package of S32K148 and selected LIN1 using LPUART0 and used SBC-UJA1131HW5V0. I am using external tool to act as a master but the slave is not responding to the headers and not getting the response send by the Master. PFA of code I am not receiving anything from l_u8_rd_LI0_Motor1Selection(). Please let me know anything I am missing or any changes required.
Please help me clarify the following:
Did the example work with the two EVBs? I would like to confirm that you were able to get the example working without making any modifications to it.
From the information provided, I understand that you are using an external tool as a master. Could you provide more information?
Hi @VaneB
First I used LIN_Master_S32k148 example with S32K148-Q176 if I use the example I am not getting any frames from the LIN interface. After making some configuration changes master is sending the frames from the LIN1. The same process I followed for slave with LIN_Slave_S32K148 and I used tool as a master that tool sends the frames using LDF file. The slave is not responding, Please let me know what is the reason I didn't modify the code.
Thanks & Regards
Bhavesh Raju
The LIN_slave and LIN_master examples are designed to work together. That is the reason you need two EVBs.
If you want to test the slave example with an external it going to need to make some changes. I do not know what tool you are using so I can not help you in that regard. The implementation in that part is up to you.