How to Measure the running time of one function on S32K344?
How to do it specifically?
Does S32DS software have a measurement function?
1
Hi @CHYYDS,
The RTD drivers have Quality packages that contains execution time of the APIs.
For example: SW32K3_RTD_4.4_R21-11_3.0.0_D2303_QualityPackage.zip
Each driver has ProfileReport.xlsx
To measure the execution time of your functions, you can use a timer or measure it externaly using GPIOs.
Regards,
Daniel
Hi @CHYYDS,
I would recommend using S32DS 3.5 and the latest RTD 3.0.0.
The RTD you downloaded is from Oct, 2021.
You need to add the .zip file as an Update side in the IDE and then install the RTD.
Once the RTD is installed, you can create a new Project from Example.
The examples show how to use the drivers.
Regards,
Daniel