MCSXTE2BK142_PMSM_FOC_1Sh build error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MCSXTE2BK142_PMSM_FOC_1Sh build error

Jump to solution
276 Views
June6
Contributor I

Hello

I installed the sw "MCSXTE2BK142_PMSM_FOC_1Sh" and found AMMClib in this SW is version 1.1.15,then I changed the AMMClib from V1.1.15 to V 1.1.19. But after building, S32DS shows the error "Description Resource Path Location Type Ld error: cannot find - lC:NXPAMMCLIBS32K14x_AMMCLIB_v1.1.19libs32ds_arm32S32K14x_AMMCLIB.a C/C++ Problem".

The configuration as below pictures,could you help me find the reason for this error?

Thank you very much!

June6_0-1719830924867.png

June6_1-1719831105842.png

June6_2-1719831122860.png

June6_3-1719831212874.pngJune6_4-1719831223363.png

 

 

 

 

 

0 Kudos
Reply
1 Solution
231 Views
VaneB
NXP TechSupport
NXP TechSupport

Hi @June6 

I have compared the changes you made to what I have and I found a discrepancy in the AMMCLIB name on C-C++ Build > Settings > Standard S32DS C Linker > Libraries > Libraries (-l). Refer to my project configuration in the attached image.

VaneB_0-1719951568018.png

View solution in original post

0 Kudos
Reply
4 Replies
242 Views
June6
Contributor I

Hi VaneB

Thank you for your support.

I checked my settings,and these settings also comply with all the suggestions mentioned in the link. But after Clean Project and Build Project, the error is still here.

June6_3-1719885334391.png

June6_0-1719885130488.png

June6_1-1719885146593.png

June6_2-1719885170424.png

 

 

0 Kudos
Reply
232 Views
VaneB
NXP TechSupport
NXP TechSupport

Hi @June6 

I have compared the changes you made to what I have and I found a discrepancy in the AMMCLIB name on C-C++ Build > Settings > Standard S32DS C Linker > Libraries > Libraries (-l). Refer to my project configuration in the attached image.

VaneB_0-1719951568018.png

0 Kudos
Reply
217 Views
June6
Contributor I
Thank you very much. It was solved.
0 Kudos
Reply
255 Views
VaneB
NXP TechSupport
NXP TechSupport

Hi @June6 

Check the following thread. It has information related to the topic that you may find useful. 

S32K116 BLDC/PMSM Motor control kit bring up

 

B.R.

VaneB

0 Kudos
Reply