Hi,
I would like to use MC33665A SYNC schedule feature to SYNC TPL1 (BCC) and TPL2 (BJB) SOC command at the same time to get the cell voltage and current measurement. Any ideas about the whole commands sequences?
Below are the sequences that I comprehend from datasheet, but not sure is correct or not?
1. config MC33665A GPIO6 as input in initial step.
2. before issue SOC command, config MC33665A SCHED_CMD. EVENT=(01)SYNC, OPERAND=1
3. issue SOC command TPL1
4. issue SOC command TPL2
5. Activated SYNC pin to high, and it with trigger MC33665A issue SOC command to TPL1 and TPL2 at the some time.
6. Read back the responses from TPL1 and TPL2.
Thanks for any advice?
Best regards,
Mark
已解决! 转到解答。
Hello,
I hope all is great with you. Thank you for using the NXP communities.
You are correct. The SYNC signal scheduling enables MC33665A to synchronize the activities such as voltage, temperature and current measurements across the battery pack working with BCC devices on TPL2 and TPL3 protocol.
I would recommend the procedure below considering that the request queue is empty:
For further information, I do recommend downloading the document below from your Secure Files. Note that such document is confidential and provided only with an active NDA number.
I hope this information helps.
Regards,
David
Hello,
I hope all is great with you. Thank you for using the NXP communities.
You are correct. The SYNC signal scheduling enables MC33665A to synchronize the activities such as voltage, temperature and current measurements across the battery pack working with BCC devices on TPL2 and TPL3 protocol.
I would recommend the procedure below considering that the request queue is empty:
For further information, I do recommend downloading the document below from your Secure Files. Note that such document is confidential and provided only with an active NDA number.
I hope this information helps.
Regards,
David